Highlighting Tier 4 Final Solutions And Connected Diagnostics™

TULARE, Calif. (Feb. 9, 2015) – Cummins Inc. (NYSE: CMI) presents its comprehensive engine lineup and latest telematics technology for agriculture customers at the World Ag Expo today through Feb. 11 in Tulare. The breadth of items on display demonstrates Cummins commitment to continue to offer the most effective and productive solutions in the agriculture industry today.

In Booths M6 and M8, Cummins will display QSB4.5, QSB6.7, QSL9 and QSX15 engines, spanning a 121 hp-to-675 hp (90-503 kW) power range for agriculture equipment meeting U.S. Environmental Protection Agency (EPA) Tier 4 Final emissions standards. There will also be three Tier 4 Final industrial power units from Cummins Power Products on display – the QSF2.8, QSF3.8 and QSG12 – ranging in power from 49 hp to 513 hp (37-383 kW). Cummins power units provide ready-to-install power for equipment such as irrigation sprayers and harvesters, and standalone power for machines such as pumps.

The QSL9 engine display will include the Cummins Emission Solutions Diesel Oxidation Catalyst (DOC) and Selective Catalytic Reduction (SCR) aftertreatment system and the Diesel Exhaust Fluid (DEF) tank and fuel lines, giving customers the chance to see a completely integrated package. To provide optimized performance for every agriculture customer, Cummins uses the right emissions technologies across different power bands, ensuring the best result for every application.

Cummins will also highlight Connected Diagnostics at the Expo. Active in over 30,000 on-highway vehicles today, and soon to be available for off-highway equipment, Connected Diagnostics is customers’ lifeline to Cummins when they need it most. Through a telematics connection, a customer’s Cummins-powered equipment wirelessly connects the engine to Cummins for immediate diagnosis of an engine system fault alert, and provides valuable information within seconds.

Cummins will also display the new ISV5.0 engine, rated from 200 hp to 275 hp (149-205 kW). Visitors to the booth will have the opportunity to see the engine both on the show floor and installed in a unique repowered 1973 Plymouth® Road Runner, also known as the Mad Maxxis Off-Road Runner. The Mad Maxxis was recently featured on the popular YouTube Motor Trend Channel show “Dirt Every Day” and at the Specialty Equipment Market Association (SEMA) show. It is one of two new engines in the V8 family, the other being the 5.0L V8 Turbo Diesel, which powers the 2016 Nissan® TITAN XD,™ on sale now.

Cummins will continue to remind farmers of the support available to them through the Cummins Care network, which allows them to tap into the largest industry service network in the United States and Canada, with over 3,200 locations. The total value that Cummins offers customers, coupled with its strong commitment to customer support, makes Cummins Care a trusted information source regarding the latest engine and product technology.

About Cummins Inc.
Cummins Inc., a global power leader, is a corporation of complementary business units that design, manufacture, distribute and service diesel and natural gas engines and related technologies, including fuel systems, controls, air handling, filtration, emission solutions and electrical power generation systems. Headquartered in Columbus, Indiana (USA), Cummins currently employs approximately 55,000 people worldwide and serves customers in approximately 190 countries and territories through a network of approximately 600 company-owned and independent distributor locations and more than 7,200 dealer locations. Cummins earned $1.4 billion on sales of $19.1 billion in 2015. Press releases can be found on the Web at cummins.com or cumminsengines.com. Follow Cummins on Twitter at twitter.com/cumminsengines and on YouTube at youtube.com/cumminsengines.