MINNEAPOLIS, Minn. (November 1, 2006) - The new ComfortGuard™ APU from Cummins is the engine manufacturer's first complete auxiliary power unit system for over-the-road trucks. The system combines the generator expertise of the company's Onan brand with tailored HVAC components to power all hotel loads for comfort and convenience.


The quiet, compact and reliable system offers an effective solution to anti-idling regulations and the high cost of diesel fuel and will be available beginning in January 2007.


"With an increase in legislation and enforcement of truck engine idling laws and the rising cost of fuel, APUs are a must for over-the-road truckers. A Cummins ComfortGuard APU system can pay for itself through reduced engine idling in about 18 months or less," says Shawn Wasson, APU business leader for Cummins. "The ComfortGuard APU system is a logical outgrowth of both the engine and idle management products for which Cummins is known, and the RV, marine and mobile generators built under the long-established Onan brand from Cummins."


The ComfortGuard system's unique plug-and-play design reduces the cost of installation by up to one-half. Quick disconnects, pre-charged A/C lines and compact dimensions allow system installation on most trucks in about a day. The system can be installed and serviced throughout the US and Canada by the extensive network of Cummins distributors and authorized dealer service locations. The ComfortGuard system reduces wear and tear on truck engines, and is designed to match the engine's oil change interval of 500 hours.


The Cummins ComfortGuard system's Cab Air™ heating and cooling components are compact and offer high performance. The space-saving A/C system fits beneath the sleeper berth and has a 12,000 Btu capacity to maintain comfortable temperatures inside the cab. The 4,000/8,000 Btu, two-stage electric heating element provides comfort in the coldest weather. The evaporator section, which also mounts under the bunk, delivers up to 350 cubic feet per minute of cool, comfortable air. Both heating and cooling are controlled by a thermostat similar to the ones found in most homes. The ComfortGuard Cab Air APU system can be programmed to start automatically based on thermostat settings or time of day.


The ComfortGuard Cab Air condenser section is contained in a heavy metal case that protects coils from road grime, rocks or gravel that can be thrown up by the tires and cause major damage. Unlike similar units that have to be mounted vertically, the ComfortGuard Cab Air condenser is designed to mount in any orientation - upside-down, right-side-up or lying flat on its back, it still delivers cool and comfortable air.


The ComfortGuard APU system is powered by a two-cylinder diesel engine - the same engine as used in many Onan RV generators where it has earned a reputation for low noise and low vibration. Equipped with a Cummins alternator, the unit produces 4,000 watts at 120 volts, 60 Hz AC, with exceptional voltage and frequency stability for sensitive appliances and electronic equipment. It also produces up to 40 amps at 12 volts DC for charging the truck's batteries, and powering lights and fans. Weighing 375 pounds, the ComfortGuard APU system is within the allowable gross vehicle weight variance for tractor-trailers equipped with APU equipment.


The unit comes standard with ground fault interrupter (GFI) outlets for added safety and to allow easy reset from inside the cab. The APU also features self-diagnostics with a built-in microprocessor and LCD readout. At the touch of a button, the operator can program automatic controls or check coolant temperature and overall operational history. The durable, powder-coated steel enclosure opens easily, providing quick access for service. Overall dimensions are 21. L x 24.5. D x 28. H, making it compact enough to mount behind fairings.


For more information about the new Cummins ComfortGuard APU, contact Ann Gougebas, Cummins, 1400 73rd Ave. NE, Minneapolis, MN, 55432. Phone: 763-574-5931; Fax 763-574-8060. Or visit www.cumminscomfortguard.com.


Cummins Inc., a global power leader, is a corporation of complementary business units that design, manufacture, distribute and service engines and related technologies, including fuel systems, controls, air handling, filtration, emission solutions and electrical power generation systems. Headquartered in Columbus, Indiana, (USA) Cummins serves customers in more than 160 countries through its network of 550 company-owned and independent distributor facilities and more than 5,000 dealer locations. The Cummins ComfortGuard™ APU system is manufactured with the expertise of the company's Onan brand. Onan mobile generators are used in the recreational vehicle, marine and fire markets, and have a long-standing reputation for quality.